PressMedia contact Would you like to be added to our media distribution list? igus® media digest |
|
| Do you have any questions? Require materials? Current news releases and printable images are available for download here. Of course, we look forward to your call, email or fax! |
|
| |
igus® keeps moving6/17/2013
igus® Inc. the world’s leading manufacturer of Energy Chains® and polymer plain bearings, is continuing its growth trend. |
|
No fuss guidance for long travels6/17/2013
igus®’ E2/000 Energy Chain® cable carriers are now available in a cost-saving design which eliminates the need for guide troughs in long travel applications. |
| |
More creative freedom for designers6/17/2013
With 80,000 machine components available from stock, polymer specialist igus® offers the right part for almost any application. Now design, maintenance and mechanical engineers who make special parts themselves can order the company’s high-performance plastics as bar stock. |
| |
New generation of micro-chains6/3/2013
igus® has given its micro cable carriers a facelift. Neat design features, such as a new double-stop dog system, make the latest E2 Micro chain even sturdier and quieter than its predecessors. |
| |
Design meets function. igus® receives prestigious product design award5/13/2013
igus®, a leading developer of high-performance polymer machine components, won two awards as part of this year's iF product design competition. |
| |
Linear actuators developed for high-speed applications with low loads4/22/2013
DryLin® ZLW belt driven linear actuators are a low-cost, short lead-time alternative to traditional re-circulating ball bearing systems. igus® DryLin products are engineered with wear-resistant, dry-running, oil-free linear bearings which do not require any maintenance. |
| |
New adjustable retraction system for cable guidance4/4/2013
From small welding robots to large palletizing robots, cable-carrier manufacturer igus® offers cable-guidance systems for a wide range of robotic applications. |
| |
Plastic plain bearing competition1/23/2013
Plastic plain bearing specialist igus® has just launched its manus competition for the sixth time. The international competition has taken place every two years since its inception in 2003. |
| |
igus releases 2013 bearings catalog1/10/2013
igus® has released a 2013 bearings catalog for its iglide® plastic bushings, igubal® self-aligning bearings, and DryLin® linear bearings and guides. |
| |
igus Supports nation-wide student robotics competition12/10/2012
For the fifth consecutive season, igus® is a sponsor for Botball, an educational robotics program produced by the KISS Institute for Practical Robotics. |
| |
igus® Sponsors 2013 Rube Goldberg Machine Contest12/3/2012
The 2013 Rube Goldberg Machine Contest® has opened for registration to international collegiate, high school, and middle school teams. |
| |
New fire-resistant plastic bushing11/1/2012
igus®, an expert in triboplastics, has released a new polymer plain bearing that is fire retardant and classified according to UL94 with V0 standards. |
| |
Strip cables 50% faster9/25/2012
igus®, an expert in cables for automated applications, presented an intelligent solution to strip back long cable lengths quickly and easily at IMTS 2012. |
| |
Low cost long travels9/25/2012
Cable carrier specialist igus® introduced a new plastic guide profile at this year’s IMTS show in Chicago, IL. Guidelite is a lightweight and cost effective system that enables Energy Chain® cable carriers to travel over long runs without requiring a steel guide trough. |
Contacts in your location (can be on-site within 24-48 hours)
myigus myCatalogPress releasesPress contactInclude into the press distribution listigus® media digest
More than 100,000 products available! Open Mon-Fri 8:00 am - 8:00 pm EST.
No minimum order