Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Self-lubricating,
long-lasting bearings

Self-Lubricating Effect for plastic bearings

Features of iglide® plastic bushings

Every iglide® plastic bushing material possesses a set of special features making it suitable for different applications and requirements. However, all iglide® plastic bushings have certain general properties in common. They are made from materials that:

1. Can handle high loads over an extended period of time
2. Have low coefficients of friction
3. Have low wear rates resulting in a longer service life
Browse the Shop

The Self-Lubricating Effect

iglide® plastic bushing materials consist of base plastics, fibers and filling materials, and solid lubricants. These components are not applied in layers, but homogeneously compounded.

The advantage of this construction becomes clear if you consider the following:

1. The coefficient of friction, determined by the surface of the plastic bushing, should be as low as possible

2. The surface must not be pushed aside by forces acting on the plastic bushing

3. The plastic bushing should be particularly resistant to wear forces acting on its surface.

There is no universal material available that can fulfill all these tasks equally well.

base polymer with fibers and solid lubricants

iglide self lubricating bearings and bushings

The traditional solution

The traditional solution is a hard shell with a soft coating. Traditionally, every lubricated bushing works according to this principle, including a number of maintenance-free bearings equipped with special sliding layers. However, this soft sliding layer is not strong enough; with high edge loads or oscillations it is stripped away. iglide® plastic bushings function differently.

One component of the iglide® plastic bushing material acts for each function:
  • The base plastics are crucial for wear resistance
  • Fibers and filling materials reinforce the bushing so that it can withstand high forces or edge loads
  • Solid lubricants automatically lubricate the bushings and reduce friction in the system.

Discuss your project with a bearings expert

Whether you're interested in turnkey, fully assembled solutions or looking to build your own customizable project, learn more about how igus® can assist you with a solution based on your specific application and requirements.
Contact an igus® expert now
igus iglide bearings expert

components of self-lubricating plastic bushings

Integrated lubrication

The solid lubricants are embedded as microscopic particles in millions of tiny chambers in the fiber-reinforced material. From these chambers, the plastic bushings release tiny amounts of solid lubricant during movement.

They are embedded in the tiny chambers, they can not be pressed out. They are always there as soon as the plastic bushing or shaft is set in motion. They help to lower the coefficient of friction.

Base plastics and technical fibers

The radial pressure acting on the bearing is taken by the plastic base material. It provides shaft support at the contact surface. The plastic base material ensures that the solid lubricants do not receive a surface pressure that is too high. The base material is also reinforced by technical fibers or filling materials. These additional materials stabilize the bushing for applications involving continuous stress.

The start-up phase

In the initial phase, the shaft and the iglide® plastic bushing become mated to one another. During this period, the surfaces of both partners are fitted to each other. The specific load of the system lowers as the contact surfaces of the shaft and plastic bushing expand during start-up. Simultaneously, the wear rate lowers and approaches a linear curve. In this phase, the coefficients of friction continue to change, until finally assuming a value that is - for the most part - constant.

Base plastic and fibers for iglide bearings



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® SE & Co. KG/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® SE & Co. KG points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® SE & Co. KG

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302