chainflex® – welcome to the world!


Machines of all kinds are now used all over the world in a global economy. For this reason, we at igus have been paying attention to high standard-compliant manufacturing of our products for years.  
 
This means that for our chainflex cables, we have a special focus on fulfilling all directives and approval regulations of the most important worldwide standards. So, you will find the right cable for almost any requirement, worldwide: chainflex - welcome to the world!
Even if there is no clear answer to the question of what the most important approval is, a few specific, mainly geographical, characteristics must be taken into account when making any purchase decision. In Europe, only machines with a valid CE mark are allowed to be placed on the market. The fulfilment of UL guidelines or compliance with EAC/CTP plays an important role for worldwide export.
 
It enables us to offer concrete solutions for a wide range of industries, as many of our customers have additional guidelines. In the semiconductor industry, these guidelines are IPA cleanroom approvals or DNV sea certifications. DESINA requirements also often play an important role. You can find the right answer to all these worldwide challenges here: chainflex - at home anywhere in the world!

chainflex® approvals and standards

chainflex® UKCA

The UK government has stipulated that products imported into the UK (England, Wales, and Scotland) require the UKCA (UK Conformity Assessed) mark.

chainflex® CE

The European directives stipulate that only products with the CE mark may be placed on the market and put into operation.

chainflex® fungerer - garanteret og certificeret!

Vores garantiløfte er certificeret af UL

chainflex® UL AWM

Underwriters Laboratories (UL) is an independent US organisation that examines, tests, and certifies products with regard to safety.

chainflex® DNV

DNV is the certification for the maritime environment, offshore facilities, gas and oil pipelines, and onshore applications such as wind, tidal, and solar energy.

chainflex® NPFA 79

NFPA 79 - the Electrical Standard for Industrial Machinery - is part of the American National Fire Protection Association.

chainflex® DESINA

DESINA is considered the standard for the electrical, hydraulic and pneumatic installation of automated production systems and machine tools.

chainflex® RoHS

The abbreviation RoHS stands for "Restriction of (the use of certain) Hazardous Substances".

chainflex® EAC

The EAC certificate replaces the formerly valid GOST certificate and is similar to the CE marking used in Europe.

chainflex® UL Listed

The UL Listed test mark is probably the most commonly used of all. UL develops and publishes safety standards

Cables in the cleanroom

Cables in the cleanroom

chainflex® REACH

REACH stands for Registration, Evaluation, Authorisation, and Restriction of Chemicals.

Worldwide success stories from our chainflex cable customers


Further information

chainflex® test lab

Tested on a floor area of 3,800m²

Two billion annual test cycles for guaranteed safety against failure.

Available in 24hrs from stock

chainflex® works: World's No. 1 for moving applications