igus® - high-quality
soldering operations ready to go
Free white paper

What exactly is meant by soldering?

Soldering is a thermal procedure that creates a non-detachable connection between materials by means of a solder.
The solder consists of tin and other metals, such as copper or silver, and is an easily meltable metal alloy that serves as connector between the materials. To connect two metal components, soldering tin is melted and applied to the stranded wire.
The solder connection technology is flexible and focusses particularly on one requirement: reproducibility. The quality depends on different parameters - e.g. on the constant temperature, the solder used or the size of the components. Hence, the contacting galvanised by hand varies. We at igus would like to realise solder connections at a constant level - by means of professional soldering stations.

Frequently asked questions


▲ Tech up

What soldering methods are there?

Soldering methods are divided to different aspects (according to DIN 8505). There are two kinds of soldering: soft-soldering and hard-soldering. With soft-soldering, the liquidus temperature of the solders is below 450°C. With hard-soldering, the liquidus temperature of the solders is between 450 and 900°C. Usually, hard-soldered connections are more mechanically stable than soft-soldered connections.

Why manual solder connections are good, but technically supported ones are better

How to increase quality and safety even in manual work

For creating electric connections, both crimp and solder connections are suitable. The latter are usually favoured, when it is necessary to ensure constant electric conductivity over a long period of time or the connection point has to be permanently sealed. 
 
But be careful: you have to know what you're doing when soldering. What might look easy at a first glance, turns out to be a complicated process that you need to master. The white paper describes the most significant mistakes during the production of solder connections. It uses the example of harnessing of cable and energy supply systems to explain why technology-supported solder connections should be given preference to manual ones in industrial environments.
 
Furthermore, the paper describes the economic advantages that the reproducibility of soldering results offers. It concludes with the risks of manual soldering for people and material, and how to minimise them.
 
Download white paper now

Advantages of the machine-supported soldering Professional soldering station at igus readychain

What are the advantages of machine-supported soldering?

If machine engineers and system integrators cannot rely entirely on crimp connections, they have to pay special attention to the quality of the solder connections. That is the only way to ensure constant electric conductivity over a long period of time and to permanently protect the connection point, e.g. against gases or liquids.
 
There are further advantages of machine-supported soldering:
  • Reproducible quality
  • Increased security at the work place due to integrated extraction systems

Quality will win!

Practical readychain application examples


▼ Cost down

Quick glance into the readycable production

Advantages of industrial harnessing

The world's No. 1 when it comes to drive cables that are suitable for use in chains

The igus readycable range extends from a large variety of cables in accordance with the standards of various manufacturers such as Siemens, SEW or Beckhoff, to cables for video/vision equipment and harnessed Ethernet cables up to CAT7. You can realise the following cost advantages with every single cable:
  • Ready-to-connect directly from the cable manufacturer
  • Up to 7 price classes with the same electrical properties
  • Exactly in the desired length (cut with cm accuracy)
  • No minimum order value or quantity
  • Ready to ship in 24 - 48 hours
  • Special forms of harnessing are part of our everyday business

Why our products keep delivering what they promise

UL verified: igus® receives the highest recognition by globally recognised testing organisation

We confidently issue a 36-month guarantee on our cables, as we are able to make reliable predictions about the service life of our cables and the ready-to-connect harnessed end systems, due to over 30 years of experience in our 3,800m² test laboratory and 700 concurrently undertaken experiments.
 
We are now the first German firm to have this promise validated for our cables. In a complex certification process, the US "Underwriters Laboratories" institute confirmed the accuracy of the "igus® 36-month chainflex® cable guarantee and service life calculator based on two billion test cycles per year" promise. This makes our Cologne-based company the first in Europe to have the veracity of an advertising statement confirmed by a testing institution. In future, every chainflex cable that leaves the factory anywhere in the world will be identified by the UL marketing label with its unique number (B129699), referring to igus.
 
These statements about the igus quality create reliability and planning security for your entire investment process; all the more so now that they have been confirmed by an external body! You can read everything about UL verified and the corresponding certification process here for free:

Tech up, Cost down

We will show you solutions for saving up to 88% assembly time, reducing weight by up to 48% or avoiding storage costs altogether.
 
Determine your individual savings potential and the optimum solution when it comes to improving technology and saving costs.
Discover individual savings potential now

Go to the products here:

Industrial connector

High-performance plug-in connectors, signal plug-in connectors and several thousand connector components – igus provides a high level of availability with short delivery times.

Cables sold by the metre

Cables sold by the metre for moving applications in energy chains: chainflex meets all requirements for electromagnetic compatibility as well as the standards and guidelines such as UL, CSA, EAC and much more.

Ready-to-connect drive cables

Offering around 4,600 harnessed motor, servo, signal and encoder cables, igus is the world's No. 1 when it comes to harnessed cables for use in energy chains.  

Ready-to-install energy supply systems

Harnessed energy supply systems from a single source: save up to 80% of process costs with our igus readychain offers.  


Konsultation

Jeg vil med glæde besvare dine spørgsmål personligt

Levering og vejledning

Personlig betjening:

Mandag til fredag fra 7:00 til 20:00.
Lørdag fra 8:00 til 12:00.

Online:

24h